TC358749XBG调试mipi_csi2寄存器全为0

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

TC358749XBG调试mipi_csi2寄存器全为0

1,011 Views
857849964
Contributor I

当我加载TC358749XBG驱动时mipi_csi2寄存器发生如下变化,在调用mipi_csi2_disable中的clk_disable_unprepare(info->dphy_clk);后mipi_csi2的寄存器全变为0,想知道是什么原因会导致这种情况呢?

MIPI_CSI2_VERSION =  0x3130302A
MIPI_CSI2_N_LANES =  0x00000001
MIPI_CSI2_PHY_SHUTDOWNZ =  0x00000001
MIPI_CSI2_DPHY_RSTZ =  0x00000001
MIPI_CSI2_CSI2_RESETN =  0x00000001
MIPI_CSI2_PHY_STATE =  0x00000300
MIPI_CSI2_DATA_IDS_1 =  0x00000000
MIPI_CSI2_DATA_IDS_2 =  0x00000000
MIPI_CSI2_ERR1 =  0x00000000
MIPI_CSI2_ERR2 =  0x00000000
MIPI_CSI2_MASK1 =  0x00000000
MIPI_CSI2_MASK2 =  0x00000000
MIPI_CSI2_PHY_TST_CTRL0 =  0x00000000
MIPI_CSI2_PHY_TST_CTRL1 =  0x00001414
MIPI_CSI2_SFT_RESET =  0x00000000


mipi_csi2_disable:130


MIPI_CSI2_VERSION =  0x00000000
MIPI_CSI2_N_LANES =  0x00000000
MIPI_CSI2_PHY_SHUTDOWNZ =  0x00000000
MIPI_CSI2_DPHY_RSTZ =  0x00000000
MIPI_CSI2_CSI2_RESETN =  0x00000000
MIPI_CSI2_PHY_STATE =  0x00000000
MIPI_CSI2_DATA_IDS_1 =  0x00000000
MIPI_CSI2_DATA_IDS_2 =  0x00000000
MIPI_CSI2_ERR1 =  0x00000000
MIPI_CSI2_ERR2 =  0x00000000
MIPI_CSI2_MASK1 =  0x00000000
MIPI_CSI2_MASK2 =  0x00000000
MIPI_CSI2_PHY_TST_CTRL0 =  0x00000000
MIPI_CSI2_PHY_TST_CTRL1 =  0x00000000
MIPI_CSI2_SFT_RESET =  0x00000000

Labels (3)
Tags (1)
0 Kudos
4 Replies

715 Views
jimmychan
NXP TechSupport
NXP TechSupport

So you disable the clk? then read the value of register is zero ?

0 Kudos

715 Views
857849964
Contributor I

官方代码都是disable的,而且在我们其他项目里面也是有disable clk的操作,但是他们操作完了之后还是能正常读取寄存器的值

0 Kudos

715 Views
jimmychan
NXP TechSupport
NXP TechSupport

I think you should not disable the clock if you want to read the value from the register.

0 Kudos

715 Views
857849964
Contributor I

我在官方代码上在dts中把fb1的hdmi输出disable后就会出现这种情况,当我把他okay后,就能正常读取寄存器,不知道这两者有没有实际联系,我在代码上是没有看到任何联系的,可以的话,麻烦指点一下!谢谢!

0 Kudos