iMX RT1064 - LPSPI Maximum FIFO Size

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX RT1064 - LPSPI Maximum FIFO Size

Jump to solution
1,078 Views
nbgatgi
Contributor IV

I was reading through the datasheet regarding LPSPI registers and found where the FIFO size is set.  The "parameter register (PARAM)" has two 8-bit fields that represent "maximum number of words in the receive FIFO, which is 2^RXFIFO" or "2^TXFIFO".  As I read this, it implies an unreasonably large maximum FIFO size.  The default value for both TX and RX is 4 which is a FIFO size of 16 words.

Looking further, the "FIFO control register (FCR)" includes 4-bit fields for FIFO watermark values.  This allows for a maximum watermark value of 15.

So, simple question:  Is the maximum LPSPI FIFO size for the RT10xx 16 words?

1 Solution
894 Views
jeremyzhou
NXP Employee
NXP Employee

Hi Nick Guzzardo,

Thank you for your interest in NXP Semiconductor products and
for the opportunity to serve you.
Q1)  Is the maximum LPSPI FIFO size for the RT10xx 16 words?
-- Yes, it's.


Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

View solution in original post

1 Reply
895 Views
jeremyzhou
NXP Employee
NXP Employee

Hi Nick Guzzardo,

Thank you for your interest in NXP Semiconductor products and
for the opportunity to serve you.
Q1)  Is the maximum LPSPI FIFO size for the RT10xx 16 words?
-- Yes, it's.


Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------