AnsweredAssumed Answered

Binary or Object file not generated with Motor Control Toolbox

Question asked by Anu Mathew on Jun 25, 2019
Latest reply on Jul 10, 2019 by Anu Mathew

Hi,

 

I am using NXP's Motor Control Development Toolbox for MPC564xL to build a simple application on MPC5643L microcontroller. I have done compilation and then build the model in Simulink. However the .elf file which is the target file is not generated in the target folder . I am using CodeWarrior compiler. I am attaching screenshots of my configuration block and my model. I have also tried the example projects. But same problem exists.

 

This is my hardware target parameters that I have configured.

 

 

Could anyone help me identifying the issue? Thanks in advance for your response.

mpc56xx codewarrior v11.0 motorcontroltoolbox mpc5643l bam

Outcomes