AnsweredAssumed Answered

EXT_SYNC of PWM initial frequency settings

Question asked by Kien Francis Ureta on Jun 22, 2019
Latest reply on Jun 23, 2019 by xiangjun.rong

Hi guys,

 

Based on NXP App note, AN4885 - eFlexPWM. The Current Reset PWM can be used using EXT_SYNC. How can I be able to change its initial frequency? The frequency in my PE settings which is shown below is not used in the PWM when there's no input signal(coming from the EXT_SYNC signal). It says in the app note code, that the initial frequency can be configured. But how?

 

 

Thanks

Outcomes