AnsweredAssumed Answered

MCUXpresso 11.0 Image Info cannot analyze build artifact

Question asked by Lucas Magasweran on Jun 21, 2019
Latest reply on Sep 4, 2019 by LPCX presso support

I'm trying to use the new Image Info feature introduced in version 11.0 but it says "Cannot analyze build artifact (/path/to/{Debug,Release}/image.{elf,axf}).

 

Analyzing the build artifact for an SDK example project does work however.

 

The only difference I could see are two extra linker options "-Xlinker --sort-section=alignment" and "-Xlinker --cref" but adding them had no effect on this issue. The both build have the same compiler options (e.g. "-fstack-usage").

 

The issue appears to be due to the location of the project. My project is stored outside the workspace directory, whereas the imported example is store inside the workspace directory. If I copy my project's build artifact to the SDK example, I can analyze it. Similarly, if I copy the SDK example's build artifact to my project outside the workspace folder, it fails with the error above.

 

How do I fix this?

relative path:

absolute path:

Outcomes