#HDLC MPC8260 Example communication
Hi guys,
I need to make an apllication in c# or c++ to communicate with
an MPC8260 with HDLC protocol via serial port .
Do I need any API from NXP ?
Do you have any example?
thanks in advance
Have a great day,
Do you you mean a bare metal application running on MPC8260 based board? There was Netcomm api by Freescale in C for such applications. I do not see any link to it on the nxp site. However you can create technical case with request for it (see How I could create a Service Request?). I also attached simple example of using the SSC as HDLC controller. It contains useful header file which describes Internal Memory Maps for the MPC8260 as C structure.
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
HI Serguei,
I will try to explain better :smileyhappy:
I have a computer with windows 10 iot entreprise that must communicate with a MPC8260 board using HDLC serial protocol.As HDLC protocol use to be vendor specific i need to know if there is any api ,lib or header from NXP to develop my windows app
thanks in advance
Sorry, I did not see any api, lib or header from NXP to develop windows app for windows OS10 iot entreprise computer.