PTN3460:
What is the max resolution for single LVDS bus mode?
Hello Michael,
Please accept my apologies for the delayed response.
PTN3460 single LVDS bus supports up to 112 MHz pixel clock, so PTN3460 can support any resolution as long as it is required less than 112 MHz pixel clock. The resolution supported is up to 1280x1024 @ 60Hz.
We do provide some VESA standard resolution table (10.1 Display resolution) in PTN3356 datasheet that you can refer to it, or you can go to VESA website (www.vesa.org) to download complete VESA timing list (need VESA member to be able to download it).
I hope this can be helpful.
Have a great day,
Paulina