Hello.
We have placed a master on the A side of the PCA 9517 ADP and a slave on the B side.
Slaves are devices that perform clock stretching.
When SCLB is 0.5 V, when the slave performs clock stretching, does both drivers start and latch up?
Hello Masaru Tamai,
First please accept my apologies for the delayed response.
Please note that for any arbitration or clock stretching it is required that the Low level on B side at the input of the PCA9517 needs to be 0.4V or below (VIL) in order to be recognized by the device and be transmitted to the A side.
I hope this can be helpful. Please let me know if you have further questions.
Have a great day,
Paulina
Hello Paulina,
Thank you for your response.
When the slave is clock stretching, the voltage on B side has dropped to 0V. At this time, is the output driver to the B side disabled?
We are concerned about the bus conflict.
Best Regards,
Hello,
It should not be disabled as per the value should be 0.4v or below (VIL and VILC in table 5) for clock stretching.
Have a great day,
Paulina