Hi,
We're using i.MXRT1051 in our project. Because of boot source some fuses needed to be burned. Those are:
- BT_FUSE_SEL @0x06
- eMMC_BOOT @ 0x05
- eUSDHC_BOOT @ 0x05
- Default_FlexRAM_Part (1011) @ 0x2D - 448KB DTCM, 0KB ITCM, 64kB OCRAM
And now uC can't boot Serial Downloader. We get:
---===>Device Information<===---
ConnectionStatus: FailedEnumeration
Current Config Value: 0x00 -> Device Bus Speed: High (is not SuperSpeed or higher capable)
Device Address: 0x00
Open Pipes: 0
*!*ERROR: No open pipes!
===>Device Descriptor<===
*!*ERROR: bLength of 0 incorrect, should be 18
bLength: 0x00
bDescriptorType: 0x00
bcdUSB: 0x0000
bDeviceClass: 0x00
*!*ERROR: Device enumeration failure
And here's the question - is it possible that reconfiguration of FlexRAM affected Serial Downloader ?
Please help,
Thanks in advance - Lukasz
Thank you for your interest in NXP Semiconductor products and
for the opportunity to serve you.
I'd like to know whether you try to use the UART interface to contact the MCU, as the Serial Downloader also supports the UART interface.
And you also can try to add a pull-up resistor to the UART_RX pin, otherwise, floating the pin may interfere with the USB enumeration process.
Have a great day,
TIC
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------