I'm the ICT engineer, now have the problem with Device U49: MCIMX6D5EYM10ADR, the JTAG not working properly in ICT(u49_u49_dis).
the bsdl file I downloaded from the website: IMX6D_21x21_BSDL_TO1.2.bsdl.
also check all power pin with U49, all OK.
on the other side, I also put the compliance pin as below to 011
attribute COMPLIANCE_PATTERNS of IMX6D: entity is
"(TEST_MODE, JTAG_MOD, POR_B) (011)";
So, I want to know, is there any more signal /pattern should be add to the device, so that can enter the JTAG model well. thanks!
Gavin
Hello,
According to Table 2-21 (Recommended connections for unused analog interfaces )
of https://www.nxp.com/webapp/Download?colCode=IMX6DQ6SDLHDG
PCIE_VP, PCIE_VPH, PCIE_VPTX (and all the other supply voltages) must remain powered
if boundary scan test (BSDL) needs to be done. Please check it.
Regards,
Yuri.