AnsweredAssumed Answered

8MM EVK board exposed pins(J1003)

Question asked by mike malgin on Jun 17, 2019
Latest reply on Jun 18, 2019 by mike malgin

Hello, 

 

I'm working with iMX8MM EVK under android 9. On the EVK board J1003 there are several exposed pins -   "EXP_IO12 5", "EXP_IO11 5", etc. Is it correct to say that I can only access these through the I2C MUX interface? Is there a way to export them and have access to these as  normal GPIOs?

 

In addition, I cannot locate any "normal" GPIOs that are being exposed through the J1003, which is very strange. Any clarification will be highly appreciated. 

 

 

Thanks! 

Outcomes