mcimx8mq-evk usb usb1-port1: connect-debounce failed

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

mcimx8mq-evk usb usb1-port1: connect-debounce failed

1,847 Views
kieuvietdich
Contributor II

Hi,

I have a MCIMX8mq-evk with manually build `linux-rel_imx_4.14.78_1.0.0_ga` version. Everything work fine exclusive usb port. I connect HID keyboard into J903, it's not work. When i run dmesg command, get "usb usb1-port1: connect-debounce failed".

Any advice for me, thanks very much.

Tags (2)
2 Replies

1,607 Views
igorpadykov
NXP Employee
NXP Employee

Hi Kieu

one can try with Demo Images from

i.MX Software | NXP 

for custom building use documentation in Linux L4.14.98_2.0.0 Documentation

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

1,607 Views
kieuvietdich
Contributor II

Hi Igor,

Demo work everything fine. Issue only come with my custom image.

I'm building Yocto image on Archlinux very much package error. I think Yocto not support Archlinux, right?

Best regards

0 Kudos