目前使用I.MX6D方案需要确认,在该方案上从图像采集MIPI-CSI接口到HDMI接口显示输出延迟时间数据是好多?有没有具体的测试数据?
Hello Huang,
From capturing image to HDMI display, the delay time of this process depends on operating system, .
for example, for Linux and Android systems, the delay time is different. Therefore, we do not have relevant data.
If the customer's application is special, he can use a real-time operating system ,such as vxworks, Or test whether Linux or Android meets his requirements.
从采集图像到HDMI显示出来,这个过程的延迟时间,取决于使用什么类型的操作系统,比如,对于linux系统和android系统,延迟的时间是不同的。因此,我们没有相关的数据。如果客户应用于特殊的场所,对延迟有一定的要求,他可以使用类似vxworks的实时操作系统。或者针对他的要求,测试linux或者android是否满足他的要求。
Have a nice day!
BR,
Weidong