MPC5748G_EMIOS_IC/OC

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC5748G_EMIOS_IC/OC

984 Views
gangzhou
Contributor II

hello,

Recently,I use mpc5748g dev kit.I want to  use emios_0 port 6(PA[6]--E0UC_6_G)as single output compare and

emios _1 port 28 (PC[6]--E1UC_28Y)as single input capture.And ,config the interrupt for port 28 . It does not work.But,it can work normally when the port config PWM output mode.How should I do?b55689

Labels (1)
0 Kudos
3 Replies

824 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi,

there should not be an issue to program this modes for pins you mentioned.

So what is the behavior you see?

Can you share a config you have?

BR, Petr

0 Kudos

824 Views
gangzhou
Contributor II

Ok,my config program below:

init_saic_saoc
{
eMIOS_0.MCR.B.GPREN = 0; /* Disable global pre-scaler (reset default) */
eMIOS_0.MCR.B.GPRE = 79; /* Divide 80 MHz clock to module by 80 */
eMIOS_0.MCR.B.FRZ = 0; /* No Freeze channel registers in debug mode if channel FREN=0 */
eMIOS_1.MCR.B.GPREN = 0; /* Disable global pre-scaler (reset default) */
eMIOS_1.MCR.B.GPRE = 79; /* Divide 80 MHz clock to module by 80 */
eMIOS_1.MCR.B.FRZ = 0; /* No Freeze channel registers in debug mode if channel FREN=0 */

eMIOS_UC_0.UC[23].C.R = 0x0; /* Disable channel pre-scaler (reset default) */
eMIOS_UC_0.UC[23].C.B.UCPRE = 0; /* Pre-scale channel clock by 0+1=1 */
eMIOS_UC_0.UC[23].C.B.UCPREN= 1; /* Enable pre-scaler */

eMIOS_UC_0.UC[6].C.B.BSL = 0;
eMIOS_UC_0.UC[6].C.B.EDPOL = 1;
eMIOS_UC_0.UC[6].C.B.EDSEL = 1;
eMIOS_UC_0.UC[6].C.B.MODE = 0x02;/*SAOC*/
SIUL2.MSCR[PA6].B.SSS = 1; /* Pad PA6: Source signal is E0UC_23_X */
SIUL2.MSCR[PA6].B.OBE = 1; /* Pad PA6: OBE=1. */
SIUL2.MSCR[PA6].B.SRC = 3; /* Pad PA6: Full strength slew rate */


eMIOS_UC_1.UC[23].C.R = 0x0; /* Disable channel pre-scaler (reset default) */
eMIOS_UC_1.UC[23].C.B.UCPRE = 0; /* Pre-scale channel clock by 0+1=1 */
eMIOS_UC_1.UC[23].C.B.UCPREN= 1; /* Enable pre-scaler */
eMIOS_UC_1.UC[28].C.B.BSL = 0;
eMIOS_UC_1.UC[28].C.B.EDPOL = 1;
eMIOS_UC_1.UC[28].C.B.DMA = 0;
eMIOS_UC_1.UC[28].C.B.FEN = 1;
eMIOS_UC_1.UC[28].C.B.IF = 2;
eMIOS_UC_1.UC[28].C.B.FCK = 0;
eMIOS_UC_1.UC[28].C.B.MODE = 0x03;/*SAIC*/
SIUL2.MSCR[PC6].B.SSS = 2; /* Pad PC6: Source signal is E0UC_23_X */
SIUL2.MSCR[PC6].B.IBE = 1; /* Pad PC6: IBE=1. */
SIUL2.MSCR[PC6].B.SRC = 3; /* Pad PC6: Full strength slew rate */

INTC.PSR[736].B.PRC_SELN = 0x4; /* IRQ sent to Core 1 */

INTC.PSR[736].B.PRIN =0x03;

eMIOS_0.MCR.B.GPREN = 1; /* Enable global pre-scaled clocks */
eMIOS_0.MCR.B.GTBE = 1; /* Enable global time base */
eMIOS_1.MCR.B.GPREN = 1; /* Enable global pre-scaled clocks */
eMIOS_1.MCR.B.GTBE = 1; /* Enable global time base */

}

0 Kudos

824 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi,

- if you want to use ch23 as counter A bus you need to set the MCB mode for it. So use 

eMIOS_UC_0.UC[23].C.B.MODE= 0x50;   // set MCB mode  

eMIOS_UC_1.UC[23].C.B.MODE= 0x50;   // set MCB mode

- comment SIUL2.MSCR[PC6].B.SSS setting. This is used for output functionality setting. For PC6 pin setting as input you need to set IMCR register to route PC6 to eMIOS1 ch28

SIUL2.IMCR[576-512].B.SSS = 2;   /* E1UC_28_Y: connected to pad PB3 */

BR, Petr

0 Kudos