Hi!
I am using an NXP-824 to drive a radio device. The device does not have any register addresses defined, and wants to just send a group of bytes based on a function code (which is not in the right place to pretend to be a register address) and I cannot seem to get the API to not try to send the register address to the device.
Is it possible with the standard API?
Is there a modified version of the API that is without subaddress?
A bit of googling suggests that others have hit this snag, so I am hoping one of you has some advice.
Thanks!
-BenBurch
BTR Controls, Inc.
Hello Ben,
My name is Sabina and I will be assisting you. In order to provide a more accurate solution I will need more information. I would like to confirm first if the NXP device you are using is in fact the LPC824.
1. Are you using any of the examples we provide?
2. Can you specify the communication protocol that your radio device supports? I ask this, because it seems strange that if the radio device supports I2C that it does not have an address associated.
Let me know this information, so I can continue to help you.
Thank you and have a great day!
Sabina