mcux sdk components

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

mcux sdk components

650 Views
henning1
Contributor I

Hi

I am working with the k64f freedom board in mcuxpresso with sdk 2.5. In the example code there is this folder called components. I find myself unable to create a new sdk project with these components, and I have also been unsuccessfull in finding the documentation related to their use. (except the docstrings in the headers)

They are not selectable from the list of libraries etc. that is included in the project creation, and the only "components" that is included by default is serial_manager and uart. I would like to play around with the other "components" as well.

Are they supposed to be just drag and dropped from the zip archive into the project folder, or is there a more correct way to use them in a project with the correct defines etc.?

Picture related.

0 Kudos
1 Reply

541 Views
danielchen
NXP TechSupport
NXP TechSupport

Hi Henning:

NXP released SDK_2.6.0_FRDM-K64F. I would suggest you try to download it from below link

https://mcuxpresso.nxp.com/en/select 

and try it again.

Regards

Daniel

0 Kudos