Does LPCScrypt work with the LPC540xx series chips? If so, where is the hdr file or how can it be built for that chip?
Hi
LPCScrypt can work with LPCScrypt board, but it is used to update on board debug firmware. see this thread of how to use it:
LPC54608 board doesnt see any debug probes
If you want to build and debug code, please use MCUXpresso IDE, it's free of charge.
MCUXpresso IDE|Eclipse-based Integrated Development Environment (IDE) | NXP
Have a great day,
Jun Zhang
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------