S32K Crystal Drive, Gain Control

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K Crystal Drive, Gain Control

Jump to solution
1,094 Views
patricklanglois
Contributor II

Hi,

Looking at the datasheet, reference manual and application notes for the S32K microcontrollers, I can't understand if there is a minimum automatic gain control additionally to the programmable one (HI/LO gain) for an external crystal drive (SOSC).

To be as clear as possible...

For each range of crystal frequencies "covered" by each of both manual gain settings, is there some automatic control that will increase the crystal drive to provide a proper level of response on the inverter input?

Regards.

1 Solution
975 Views
jorge_a_vazquez
NXP Employee
NXP Employee

Hi Patrick Langlois

Yes, there is an automatic control that will do this internally, customer has to connect the external resistors based in the crystal manufacture specifications.  When high gain is selected, provides better noise immunity but does draw/ higher current, with low gain power consuption will be lower and customer can see a smaller signal in the pins due to the power saving.

Regards

Jorge Alcala

View solution in original post

1 Reply
976 Views
jorge_a_vazquez
NXP Employee
NXP Employee

Hi Patrick Langlois

Yes, there is an automatic control that will do this internally, customer has to connect the external resistors based in the crystal manufacture specifications.  When high gain is selected, provides better noise immunity but does draw/ higher current, with low gain power consuption will be lower and customer can see a smaller signal in the pins due to the power saving.

Regards

Jorge Alcala