Hello,
In the i.MX8M Mini EVK hardware user guide, section 3, table 8 shows the stackup as:
Figure 1
In the PCB layout file, the stackup is shown as:
Figure 2
What is the reason for difference in some of the layer thickness? Also, is it safe to assume, the PCB layout stackup (Figure 2) is the correct one?
Thanks,
Faiz
Hello,
The correct one should be the figure 2,
the figure 1 is just a guideline of how the board could be made.
Hope this helps,
Best regards,
Aldo.
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------