iMx8 eVB for automotive applications

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMx8 eVB for automotive applications

638 Views
engineer_embedd
Contributor I

Hi,

Presently we are using iMX6Q (MCIMX6Q6AVT10AC) processor for vehicle infotainment based on SABRE Auto  development board.

we want to use iMX8 processor for the same application.Is it Possible..?

Can anyone suggest iMX8 SABRE AUTO eVB..? Also processor part no..?

How to port from iMX6Q to iMX8 Quad processors..

Pls help..

thanks and regards 

Divya

0 Kudos
1 Reply

537 Views
CarlosCasillas
NXP Employee
NXP Employee

Hi Divya,

The Auto-qualified processors are i.MX8 and i.MX8X families, but they are still on preproduction stage, and no additional information/support could be provided yet. It is recommended contacting your local Sales/FAE for additional details.

In the meantime, you could take a look to the MEK boards for i.MX8 and i.MX8X at the following links:

i.MX 8 Multisensory Enablement Kit | NXP 

i.MX 8QuadXPlus Multisensory Enablement Kit | NXP 


Hope this will be useful for you.
Best regards!
/Carlos
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
-------------------------------------------------------------------------------

0 Kudos