AnsweredAssumed Answered

Can FRDM-K64F be powered from the P5V_USB pin(J3 -pin10)?

Question asked by Anders Gjeruldsen on Jun 3, 2019
Latest reply on Jun 5, 2019 by Sabina Bruce

Hi,

 

I want to power the FRDM-K64F from a shield, and I was wondering if the P5V_USB can be used to power the board.

It seems to work fine, however I was wondering if there any disadvantages to use the P5V_USB pin instead of the P5-9V_Vin pin?

 

Best regards

Anders 

Outcomes