AnsweredAssumed Answered

NFS Hangs with linux 4.9.166 on IMX6Q

Question asked by Alexis Fronteau on May 31, 2019
Latest reply on Jun 5, 2019 by Alexis Fronteau

Hi, 

I have a trouble to boot in NFS a linux 4.9.166 on an IMX6Q, it hangs forever after this following lines :

[12.193345] Sending DHCP requests ., OK
[ 12.273188] IP-Config: Got DHCP answer from 192.168.1.1, my address is 192.168.1.194
[ 12.281050] IP-Config: Complete:
[ 12.284435] device=eth0, hwaddr=00:14:2d:49:e7:09, ipaddr=192.168.1.194, mask=255.255.255.0, gw=192.168.1.1
[ 12.294783] host=192.168.1.194, domain=imajing, nis-domain=(none)
[ 12.301425] bootserver=0.0.0.0, rootserver=192.168.1.211, rootpath= nameserver0=192.168.1.1

 

The configuration that I use work with a linux 3.14.52, I have done few changements to work with the new kernel version but the nfs part is still the same. Do I miss settings to add to the configuration ? 

 

Thanks

Outcomes