I have a problem with Kinetis studio, I can't share the pins because the expert mode is not settable there are only basic and advanced.
I hope you can help me, thank you very much.
Hi GABRIELE VALLESI,
Right click the pin that you want to share, and then enable it.
Best Regards,
Robin
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
----------------------------------------------------------------------------------------------------------------------
Hi Robin,
thanks a lot for the answer, but my problem is that the Pin Sharing is disabled
thank
Gabriele
Would you please tell me the part number of your MCU?
Please also show me which component of Processor Expert are used.
Best Regards,
Robin
Hi Robin,
I'm using MKE06Z128VLD4 and the component is module SPI (Kinetis/AsynchroMaster).
I use this module to send only the data to external DAC and I don't need the DIN pin.
Thank you very much for your help.
Best Regards
Gabriele
Similar problems have been discovered before: Pin sharing not allowed between Capture and BitIO component (Kinetis KE06)
Taking into account the specificity of the PTB4 pin, would you please use other SPI pins?
Best Regards,
Robin
Hi Robin,
I need to use the PB4 pin for an output but it is blocked by the SPI for the DIN signal that I don't need and that I can't disable, can you help me?
thank you very much for your help
best regards
Gabriele