AnsweredAssumed Answered

buildroot aarch64 config for g2d for i.MX8MM

Question asked by brenhale on May 30, 2019
Latest reply on May 30, 2019 by brenhale

We have buildroot setup for the i.MX8MM, and would like to add support for using libg2d, through package BR2_PACKAGE_IMX_GPU_G2D

 

However this depends on BR2_ARM_EABIHF, and hence is at odds with our aarch64 setup.

 

I see there is a year old patch that mentions only 32bit support for libg2d 
https://buildroot.uclibc.narkive.com/JOeEbB4P/patch-0-4-imx-graphics-packages-update-to-6-2-4-p1-2

 

Is this still the case? 

 

I see there are aarch64 compiled gpu drivers here (for i.MX6 and 7 according to the release notes)

https://www.nxp.com/lgfiles/NMG/MAD/YOCTO/imx-gpu-g2d-6.2.4.p4.0-aarch64.bin

 

 

Thanks

Outcomes