AnsweredAssumed Answered

WiFi Scan not working in Android Auto

Question asked by mayank sirotiya on May 30, 2019
Latest reply on Jun 3, 2019 by CarlosCasillas

Hello All,

 

I am working on iMX8QXP-CPU MEK. And I have flashed following pre-built Android Auto image downloaded from NXP portal.

android_p9.0.0_1.0.2-auto-beta_image_8qmek

I have ported my WLAN driver for this board, and able to install the module.

Using CLI, I am able to bring up my interface and connect to an AP. ping is also working fine.

 

However, I have couple of questions :-

1. I tried setting following

setprop wifi.interface <interface_name> && setprop wifi.direct.interface <interface_name>

still not able to scan available networks using GUI.

Is there is anything else I need to do for making this work?

 

2. I cannot find dhcp running in this image. Also do not know how to start this.

As a result, I have to assign ip manually.

Is there any command to start dhcp? To help resolving ip address automatically?

 

Many Thanks,

Mayank

Outcomes