Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you. It's available to use two below sets of pins to connect an external SPI device, please give a try.
------------------------------------------------------------------------------- Note: - If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored Please open a new thread and refer to the closed one, if you have a related question at a later point in time. -------------------------------------------------------------------------------
Hi Adrian Neal ,
Thank you for your interest in NXP Semiconductor products and
for the opportunity to serve you.
It's available to use two below sets of pins to connect an external SPI device, please give a try.
Pin Name Board Location
MISO J9 pin 11
MOSI J9 pin 13
PCS0 J9 pin 15
SCK J9 pin 9
Pin Name Board Location
MISO J13 pin 12
MOSI J13 pin 2
PCS0 J9 pin 3
SCK JP11 pin 2
Have a great day,
TIC
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------