Hi everyone:
I have two different devices, coordinate and end device. coordinate is zigbee 3.0 base device application note and end device is zigbee HA demo's ColorDimmerSwitch,respectively as follow:
Now i want to establish link between coordinate and end device,but i failed.
Note:These two devices use different protocol stacks
Can you give me some tips or ideas? thank you!!!
Hello Zhang, I hope you're doing well!
The Zigbee 3.0 stack and the Zigbee HA stack are compatible, so you should be able to work with a Zigbee 3.0 Base device and your HA end device.
The ColorDimmerSwitch device is acting as a commissioner of the light devices, so it can control them.
May I ask, what is your final application? If the ColorDimmerSwitch is not working out for you, I would recommend you to try with the ColorSceneController instead, included in the JN-AN-1219 application note.
Please let me know if you have any further questions.
Best regards,
Sebastian
Hi Sebastian,
As you said, the Zigbee 3.0 Base device works with HA end device well.
I just want to control an HA OnOff end device,now it works well.
Thanks you.