AnsweredAssumed Answered

Some parts of the camera frame are green

Question asked by Gavin Cho on May 27, 2019
Latest reply on May 27, 2019 by Victor Linnik

Hi,

 

My environment is i.MX8X + one MIPI-CSI2 digital camera (resolution is 2M).

I modify max9286 driver to let it support another serializer (MAX96705) and connect with another camera sensor.

When I use yavta to capture the frame, 1/3 to the right of the frame is green as below.

 

 

I want to know if i.MX8X MIPI CSI-2 can support 1080p or not.

 

PS:

From imx-yocto-L4.14.98_2.0.0_ga Linux release notes.pdf, we can see that it says MIPI CSI camera can support up to 1080p.

 

 

 

Thanks.

Outcomes