AnsweredAssumed Answered

u-boot hanging in T4160RDB-64B Machine

Question asked by vinothkumar s on May 25, 2019
Latest reply on Jun 14, 2019 by vinothkumar s

Dear NXP,

 

I am working on t4160rdb-64b machine. Porting and booting was done properly at starting stage (At 1nd DDR3 controller and few drivers. After I configured the 2nd DDR3 controller the board is hanging at u-boot. After I disable the 2nd DDR3 controller also the board is hanging in u-boot.

 

Root cause,

1, And also I load the fman firmware for ethernet. I am not sure about this binary, I download this binary from the given link,

https://github.com/NXP/qoriq-fm-ucode

 

2, Due to 2nd DDR3 Controller initialization

 

3. Due to NAND Flash Controller

 

4. Due to Hardware Problem.

 

But, I check with all scenario. Still I have the same issue .

 

 

Please check the attachment. 

 

 

 

Thanks & Regards,

VInothS

kalaiyarasan Poyyamozhi

Outcomes