AnsweredAssumed Answered

IMX8MQ M4 UART problem.

Question asked by Sivaram SR on May 24, 2019
Latest reply on Jun 15, 2019 by Sivaram SR

Hi,

 

I am using a IMX8MQ eval board from TechNexion, while playing around with the M4 Core of the SOC I noticed that in all examples provided I am not able to recieve using UART but am able to transmit without a problem.

 

I am using the SDK provided by them (SDK version 2.3)

 

I tried all UART recieve APIs but all in vain.

I checked the device tree files so as to make sure that the device tree initialization is not conflicting with what I have defined for M4 Core.

 

Link to the project

 

I even checked the hardware the UART singals are there till the SOC Pins.

I also tried changing ports but still no luck..

 

Any help would be appreciated..!!

Thanks in Advance

Outcomes