AnsweredAssumed Answered

S32K118 controllers LPUART0 module reception doesn't work via bluetooth.

Question asked by nagaprasad vasamsetti on May 22, 2019
Latest reply on May 27, 2019 by Victor Jimenez

=> I'm working with 'FS32K118' controller "EVALUATION" board. And i'm flashing the code onto the Controller using IAR IDE.

=> 'LPUART0' transmission and reception works fine with "Serial port" and "Other Controllers".

=> The UART communication via 'BLUETOOTH' when performed with other microcontrollers works efficiently, but the same "BLUETOOTH" when used with "FS32K118" evaluation board for UART Communication using 'LPUART0' module doesn't work. The transmission works but the reception doesn't work. I have tried configuring the "LPUART0" with all the possible baud rates.

=> I have used the same "BLUETOOTH" with "FS32K144" controller for "LPUART0" and it works efficiently.

=> Can you please provide with any solutions on this as soon as possible?

Outcomes