AnsweredAssumed Answered

SEGGER J-Link configurations don't show up in MCUXpresso IDE

Question asked by László Monda on May 21, 2019
Latest reply on Jun 9, 2019 by Erich Styger

Hi there,

 

I'm back to firmware development after a long break, and I've just realized that I can't flash firmware with SEGGER J-Link via MCUXpresso IDE 10.3.1 on Linux anymore.

 

Our project is open source. See the .launch files. I can see uhk60-right_debug_kboot and uhk60-right_release_kboot under External Tools Configurations, but I can't see the uhk60-right_debug_standalone_jlink configuration anywhere, including Debug Configurations and Run Configurations.

 

When I double-click on the "GDB SEGGER Interface Debugging" menu item of the Debug Configurations dialog, I get a dialog featuring:

 

"An error has occurred. See error log for more details.
java.lang.NullPointerException"

 

JLinkExe works from the command line, but I can't use SEGGER JLink from MCUXpresso IDE. Any help would be appreciated.

 

- Laci

Outcomes