Hi all,
I used the demo JN-AN-1217 to develop my own product,and i get a question when i am in finding and binding.
Here is the question,
I add 3 endpoint to router node so the node have 4 endpoint, when I use the end device as a controllor to bind with the router as a target. The first endpoint that I added and the original one were bind successed,but the others always fail to binding.
When I delete the first endpoind i add, one of the endpoint which is failed getting success to binding. I think that there are only two endpoints can be bind in this node.
But I didn't find out that somewhere to set up this. So I ask help for you .
thank you!
Hi,
Please look at the zpscfg file that the binding table supports more devices.
Could you please define the TRACE_APP_BDB in the make file? Then if the binding table is full, you will see the next print command.
case BDB_EVENT_FB_ERR_BINDING_TABLE_FULL:
DBG_vPrintf(TRACE_APP_BDB,"ERR: Bind Table Full\n");
break;
Regards,
Mario
thank you!