LS1043 support for mtd qspi

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LS1043 support for mtd qspi

2,941 Views
prodrigu
Contributor I

Is there any support for MTD QSPI in Linux?

4.1.13 version of kernel doesn't allow to use MTD partitions.

I read the kernel driver and found this list on latest kernel version:

./drivers/mtd/spi-nor/fsl-quadspi.c        Linux < 5.1

or

./drivers/spi/spi-fsl-qspi.c                     Linux > 5.1

static const struct of_device_id fsl_qspi_dt_ids[] = {
{ .compatible = "fsl,vf610-qspi", .data = (void *)&vybrid_data, },
{ .compatible = "fsl,imx6sx-qspi", .data = (void *)&imx6sx_data, },
{ .compatible = "fsl,imx7d-qspi", .data = (void *)&imx7d_data, },
{ .compatible = "fsl,imx6ul-qspi", .data = (void *)&imx6ul_data, },
{ .compatible = "fsl,ls1021a-qspi", .data = (void *)&ls1021a_data, },
{ .compatible = "fsl,ls2080a-qspi", .data = (void *)&ls2080a_data, },
{ /* sentinel */ }
};

‍‍‍‍‍‍‍‍‍‍

Does this mean that  fsl-ls1043 is not supported?

Thanks,

Pablo

Labels (1)
0 Kudos
Reply
2 Replies

2,736 Views
Pavel
NXP Employee
NXP Employee

See the Chapter 30 of the LS1043a Reference Manual:

https://www.nxp.com/webapp/Download?colCode=LS1043ARM

 

This document shows that LS1043a supports QSPI.

 

Use the following command for kernel menu under LSDK-1903:

flex-builder -c linux:custom -a arm64 -m ls1043ardb

 

or

 

flex-builder -c linux:custom -a arm64 -m ls1043aqds

 

Use the following sequence for enabling QSPI in this kernel menu:

Device Drivers  --->

                <*> Memory Technology Device (MTD) support  ---> 

                               <*>   SPI-NOR device support  --->

                                               <*>   Freescale Quad SPI controller

 

The LS1043A QuardSPI controller is the same as LS1021a QuardSPI controller.


Have a great day,
Pavel Chubakov

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply

2,736 Views
prodrigu
Contributor I

Also, I found that adding a map like file linux/ts5500_flash.c at master · torvalds/linux · GitHub 

makes the MTD work  as expected

0 Kudos
Reply