Hi, everyone, recently I tried to change physical memory address's value on my i.MX 28 EVK(with OpenWrt operating system) but kept failing.
I found that their is a "MMU" in arm926ej-s so that value were not actually write into the physical memory, so I want to disable it. According to ARM offical DOC:"To disable the MMU, clear bit 0 in CP15 c1."
I use OpenOCD and run "arm mrc 0 0 0 0",but only get a strange number and MMU didn't disable.
Any advisory can be given?
Thanks.
Hi Jack
for examples with disabled mmu one can look at i.MX28 OBDS baremetal tests
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------