Hello Everyone,
I have IMX6UL Evaluation kit. I want to program .sdcard image into sdcard and boot the board. I tried this file from NXP site fsl-image-validation-imx-imx6ul7d.sdcard and fsl-image-gui-x11-imx6ulevk.sdcard.bz2.
Program the SDcard through the command
sudo dd if=<image name>.sdcard of=/dev/sd<partition> bs=1M conv=fsync
Did the DIP changes according to internal boot and boot from sdcard.
My board is not booting and I am not getting any output on hyperterminal.
Can someone please point me what am I missing? Any help would be appreciated.
Regards,
Asma
I will try it again with the mentioned images and update you the result.
Thank you Joan.
Yes, I did that but I am getting nothing on UART and I am using sdcard images fsl-image-gui-x11-imx6ulevk.sdcard.bz2 from L4.1.15_1.1.0_ga. my evaluation board is 700-28616 REV A and SCH-28616.
Could you please check if above files support this board?
Thanks,
Asma
it seems that you dd the image to sd card failed, pls unzip "fsl-image-gui-x11-imx6ulevk.sdcard.bz2 ", try to use "fsl-image-validation-imx-imx6ul7d.sdcard"
I have tried the same. Document already mention we have to extract and then download the file onto sdcard.
I tested this for you:
1) download the "L4.14.98_2.0.0_MX6UL7D" from the link as below:
i.MX6UltraLite Evaluation Kit | NXP
2) then I dd the "fsl-image-validation-imx-imx6ul7d.sdcard" into the micro sd card
$ sudo dd if=fsl-image-validation-imx-imx6ul7d.sdcard of=/dev/sdb bs=1M && sync
3) then I insert the micro sd card, then you need to use J1901 to check output message, I can find the board boot up successfully
Hi Joan,
thank you for the reply. I have correctly set sw601 to D1,D2,D4-OFF and D3-ON and SW601 to internal boot mode. I dont see anything on UART as well. Which log file are you asking for?
set SW602 to ON OFF, the log file is the output file from uart port when you boot up the board, when you boot up the board, pls check if anything output from the uart port
did you set the correct sw601? could you see anything though the uart port? pls send the log file to me, let me double check it. you should program the "fsl-image-validation-imx-imx6ul7d.sdcard" to the microsd card by the command you attach