Hello i have a question about lwip echo(freertos or bm version is the same) i tried to sent a byte array but the receiver receive packet truncated to first 0.(not ascii character)
for example if i send {1,2,3,4,5}(dec) the receiver receive correctly {1,2,3,4,5} , the the sender send {1,2,0,4,5} receive{1,2,0,0,0} and again {1,2,3,0,5} it receive {1,2,3,0,0}. is very weird because the lenght is always correct to 5 also if the receive packet is truncated.
thanks
Hi Simone:
By default, echotool will send your pattern 5 times. 5 is the default number of attempts.
The number of attempts can be modified by /n parameter.
Please refer to my picture below. "/n 3 " means patter helloworld will be sent 3 times. As you can see, Corrupted is 0.
For better understanding your question of the truncated data, could you please attach your screen shots ?
Regards
Daniel