Hello everyone,
I am using the official MCIMX7SABRE development board. My Linux version is 4.9.88.
When I was doing serial port data transmission and testing, I found that the kernel was printing:
Alloc_contig_range: [b0900, b0914) PFNs busy
Alloc_contig_range: [b0920, b0934) PFNs busy
What is the cause of this? Is there any way to fix it?
I look forward to anyone's reply.
Hi 其东 刘
these messages are from CMA (Contiguous Memory Allocator) allocation
as for example reported on below link and one try to increase cma size
https://bugzilla.redhat.com/show_bug.cgi?id=1387793
Try latest nxp inux L4.14.98
linux-imx - i.MX Linux kernel
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------