Qt 5.12 build on Yocto 2.0.3 jethro, for imx6q

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Qt 5.12 build on Yocto 2.0.3 jethro, for imx6q

887 Views
sergei_p
Contributor III

Hello,

We have a IMX6Q BSP based on Yoct 2.0.3 Jethro, with meta-qt5 v 5.5.1. Now, we are asked to upgrade to meta-qt5 v5.12, in context of the same Yocto 2.0.3.

Is there someone who tried to upgrade to the newest meta-qt with some older IMX Yocto distributions? Is it doable?

Or should we consider from the start to switch to the latest IMX 4.14.78 first, and then try to upgrade to meta-qt5 5.12 from there?

Any thoughts are welcome.

Regards,

Sergei

Labels (3)
0 Kudos
1 Reply

676 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello Sergei,

The problem is that  QT version 5.12 does not work even in 4.14.78, you have to check it with the community.

FSL Community BSP 

Regards

0 Kudos