DRAM_SDCLK0 or DRAM_SDCLK1 need to use if we are using two DDR3L

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

DRAM_SDCLK0 or DRAM_SDCLK1 need to use if we are using two DDR3L

529 Views
sagar_kumar
Contributor I

Hi

We are using two DDR3L in our design using i.MX6 Quad. Let me know we have to use DRAM_SDCLK_0 or DRAM_SDCLK_1 of i.MX6Q to interface two DDR3L Clocks

In Sabre brd, They are using DRAM_SDCLK_0  for Data32 to Data63 and DRAM_SDCLK_1 for Data0 to Data31, Please let me know why they follow this convention and what i have to follow since i am using two DDR3L only (DATA0-31)

Labels (1)
0 Kudos
1 Reply

457 Views
igorpadykov
NXP Employee
NXP Employee

Hi Sagar

both these clocks are identical so one can use them in any combination.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos