AnsweredAssumed Answered

Coordinate select enddevice to join the network

Question asked by zhang zhaoge on May 16, 2019
Latest reply on May 21, 2019 by Mario Ignacio Castaneda Lopez

Hi, everybody

    How do we implement that coordinate to select a device that has a certain device number and then let it to join the network.

 

Scenario description:

    Assuming that there are two devices,one is coordinate and another is enddevice.Enddevice has an SN number is 123456789.

Now when coordinate creates a network and then i send SN which is 123456789 to it.(to coordinate).I can add enddevice to the network.

And I have another question:

    When coordinate and enddevice don't association,can I send broadcast data to enddevice.

    thanks!!!

 

Outcomes