AnsweredAssumed Answered

MPC5744P Chip Version

Question asked by 260068845@qq.com on May 15, 2019
Latest reply on May 21, 2019 by Constantin Razvan Chivu

Hello,

   I have a problem. When using the cycle execution code, the 2016 version of the MPC5744P chip can only perform a 50Hz cycle. If the cycle is higher than this cycle, it will not run. The same model can execute the 200Hz cycle in the 2018 version of the MPC5744P. I would like to ask if there are different places in the next two versions of the chip, thank you?

setting message

Outcomes