AnsweredAssumed Answered

A71CH: Supported Commands mismatch with Doxygen documentation

Question asked by Quentin Cabrol on May 15, 2019
Latest reply on May 28, 2019 by Kan_Li

Dear NXP Team,

 

I am reaching you regarding the A71CH functions and more specifically the documentation of the Config tool.

After playing a bit with the base functions, it seems that the option "-c 20" supposed to return the public key of a pair (with get pub) or the reference to a public key (using refpem) is not supported. This does not match with the provided Doxygen documentation.

 

What would be the correct option value then to retrieve only a public key or reference a public key of a given pair with refpem ?

 

I have attached below some screenshots of the command calls result with "-c 10" (works) & "-c 20" (fails) options.

 

Thank you in advance for your support.

 

Doxygen excerpt:

 

get pub calls:

 

 

refpem calls:

 

Outcomes