Register and Peripheral View in MCUXpresso on i.MX RT1020

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Register and Peripheral View in MCUXpresso on i.MX RT1020

Jump to solution
2,419 Views
mjbcswitzerland
Specialist V

Hi All

Does anyone know how to view registers and peripheral (registers)?

The register view is grayed out and the only way that I can presently see where the PC is operating is to use the disassembly view.

Thanks

Regards

Mark

Labels (1)
0 Kudos
1 Solution
2,177 Views
BlackNight
NXP Employee
NXP Employee

Hi Mark,

If views are 'grayed' it means that they are already open. There is no other meaning of this.

pastedImage_1.png

So you had them open, but maybe missed the view in the perspective?

I hope this hels,

Erich

View solution in original post

4 Replies
2,177 Views
BlackNight
NXP Employee
NXP Employee

Hi Mark,

I don't have a 1020 at hand, so here with the 1051 which is the same for the 1020:

Core registers:

pastedImage_1.png

Peripherals+:

pastedImage_2.png

which uses a memory rendering:

pastedImage_3.png

I hope this helps,

Erich

0 Kudos
2,177 Views
mjbcswitzerland
Specialist V

Eric

Although the register view was grayed out in the Windows -> Show View -> Other-> Debug -> Registers menu I could still click on it and then both the CPU register and Peripherals appeared.

Then I closed the two windows and the Register entry in the menu was no longer grayed out so I could re-enable the register view again normally (but it didn't this time switch in the Peripherals too).

I needed to search to re-enable the peripheral view since it is in Windows -> Show View -> Other->MCUXpresso IDE -> Peripherals+ instead.

But all seems OK now.

Thanks

Mark

0 Kudos
2,178 Views
BlackNight
NXP Employee
NXP Employee

Hi Mark,

If views are 'grayed' it means that they are already open. There is no other meaning of this.

pastedImage_1.png

So you had them open, but maybe missed the view in the perspective?

I hope this hels,

Erich

2,177 Views
mjbcswitzerland
Specialist V

Eric

You may be right.

Regards

Mark

0 Kudos