chromiom --help
FATAL:chrome_main_delegate.cc(347)] execlp failed: No such file or directory (2)
also which man
which: no man in (/usr/local/bin:/usr/bin:/bin:/usr/local/sbin:/usr/sbin:/sbin)
strace information:
execve("/usr/lib/chromium/man", ["man", "chromium"], 0xaaab08b1d030 /* 24 vars */) = -1 ENOENT (No such file or directory)
execve("/usr/local/bin/man", ["man", "chromium"], 0xaaab08b1d030 /* 24 vars */) = -1 ENOENT (No such file or directory)
execve("/usr/local/sbin/man", ["man", "chromium"], 0xaaab08b1d030 /* 24 vars */) = -1 ENOENT (No such file or directory)
execve("/usr/local/share/python/man", ["man", "chromium"], 0xaaab08b1d030 /* 24 vars */) = -1 ENOENT (No such file or directory)
execve("/sbin/man", ["man", "chromium"], 0xaaab08b1d030 /* 24 vars */) = -1 ENOENT (No such file or directory)
execve("/usr/sbin/man", ["man", "chromium"], 0xaaab08b1d030 /* 24 vars */) = -1 ENOENT (No such file or directory)
execve("/usr/local/bin/man", ["man", "chromium"], 0xaaab08b1d030 /* 24 vars */) = -1 ENOENT (No such file or directory)
execve("/usr/bin/man", ["man", "chromium"], 0xaaab08b1d030 /* 24 vars */) = -1 ENOENT (No such file or directory)
execve("/bin/man", ["man", "chromium"], 0xaaab08b1d030 /* 24 vars */) = -1 ENOENT (No such file or directory)
Dear Terry,
See the link, please!
i.MX8MM Chromium Build Crash in Yocto imx-4.14.... | NXP Community
Probably the issue you encountered was similar to it.
Hope it can help you!
Have a nice day!
BR,
Weidong