AnsweredAssumed Answered

MTRCKTSPS5744P flash code via S32 Design Studio

Question asked by Rafael Barbosa on May 14, 2019
Latest reply on Jun 25, 2019 by Rafael Barbosa

Hello,

 

Starting with the MTRCKTSPS5744P_S32DS project example from NXP on the S32 Design Studio, I could build the project, but I can not flash the .elf file into the board.

 

The configuration is the default as follows:

No port connection can be found in order to flash the code in the board.

 

Also I could connect the MTRCKTSPS5744P kit via the USB port interface to the FreeMaster with no problem.

 

How can I flash the code to the MTRCKTSPS5744P?

Kind Regards, Rafael

Outcomes