Older SDK for K66F

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Older SDK for K66F

Jump to solution
746 Views
bssachin1
Contributor I

The current version of SDK for FRDM-K66F is 2.5. However, in mbed (https://github.com/ARMmbed/mbed-os/tree/master/targets/TARGET_Freescale/TARGET_MCUXpresso_MCUS/TARGE...), the SDK version for FRDM-K66F is 2.2. The SAI code which works in SDK 2.5 does not work in SDK 2.2 in mbed and we have identified that updating SAI/SAI_EDMA drivers in mbed fixes the issues. 

Using the SDK building, I am only able to access SDK 2.5. We were planning to release some code with mbed so that it is easier for others to use. But, since the SAI code didn't from the newer version didn't work directly, I wanted to look at example code from SDK 2.2 and change the code accordingly. Could you tell me how to get an older SAI example from SDK 2.2 for K66F? 

1 Solution
649 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Sachin BS,

I download and upload it to google drive, please try to  get it :

https://drive.google.com/open?id=1VrSEJOH5ofGp29bU3s8U18Mnx1quS37P 

Hope it helps,


Have a great day,
TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

View solution in original post

3 Replies
649 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Sachin BS,

When download SDK package, we can also choose the old version:

pastedImage_37.png

so you can download the SDK2.2 for FRDM-k66 from the below link:
https://mcuxpresso.nxp.com/en/dashboard?uvid=172015     

You can also refer to your requirement config options and download.

Hope it helps,


Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
649 Views
bssachin1
Contributor I

Hi Alice,

Using the link (https://mcuxpresso.nxp.com/en/dashboard?uvid=172015), I get the following error.

link error.png

I didn't see any link for SDK version in SDK builder

SDK builder screenshot.png

0 Kudos
650 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Sachin BS,

I download and upload it to google drive, please try to  get it :

https://drive.google.com/open?id=1VrSEJOH5ofGp29bU3s8U18Mnx1quS37P 

Hope it helps,


Have a great day,
TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------