AnsweredAssumed Answered

Imx6ul spi clock interval

Question asked by jiehuai zhu on May 14, 2019
Latest reply on Jul 24, 2019 by Dahyun Kim

Hello!

   I am using imx6ul

   The kernel version is linux4.1.15

   I configured the device tree and kernel and tested it with Documentation/spi/spidev_test.c

   However, I set up an 8-bit transfer. After the clock has finished transmitting the 8-bit byte, there will be a time interval and then the clock will be sent. As shown below, I should modify it there to modify the size of the interval.

Outcomes