Can the currently used flash bank be determined?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can the currently used flash bank be determined?

579 Views
mario_goeckel_e
Contributor I

i want to write data of a new software-image via IAP (In Application Programming) to this one of flash-banks (A and B), which is currently NOT in use to not run into conflict with parts of the running application located on the currently used flash-bank.

Within the user-manual of LPC43xx i only found the command "Chip_IAP_SetBootFlashBank(..)" for setting the boot flash-bank to A or B.

But what I need is to evaluate the used flash-bank (e.g. A) in the first place and set the boot flash-bank (B) in the second place.

0 Kudos
2 Replies

494 Views
jeremyzhou
NXP Employee
NXP Employee

Hi Mario Göckel,

Thank you for your interest in NXP Semiconductor products and
for the opportunity to serve you.
To be honest, I'm a bit confused with the mean of 'what I need is to evaluate the used flash-bank (e.g. A) in the first place'.
Whether you want an indicator to tell which flash bank is active now, please explain it.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos

494 Views
mario_goeckel_e
Contributor I

Hello and thanks for the fast response,

Yes, i need an indicator, which tells me which flash bank is active.

Here i already found FLASHCFGA, FLASHCFGB and i am reading bit31 of these registers.

Of cource i could have written a function and a function pointer, pointing to this function and just reading this address to know which flash bank is used, but this would only be a workaround.

I guess this issue can be closed now.

Best regards

Mario Göckel

Von: jeremyzhou

Gesendet: Dienstag, 14. Mai 2019 04:16

An: Goeckel, Mario (ext) (SHS PV R&D-PE MDGC)

Betreff: You have been mentioned by jeremyzhou in Re: Can the currently used flash bank be determined? in NXP Community

NXP Community <https://community.freescale.com/resources/statics/1000/35400-NXP-Community-Email-banner-600x75.jpg>

You have been mentioned

by jeremyzhou<https://community.nxp.com/people/jeremyzhou?et=notification.mention> in Re: Can the currently used flash bank be determined? in NXP Community - View jeremyzhou's reference to you<https://community.nxp.com/message/1150794?commentID=1150794&et=notification.mention#comment-1150794>

0 Kudos