imx6 q Crash and black screen

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx6 q Crash and black screen

978 Views
897122694
Contributor I

There is a system:IMX6 Q+2GB DDR+32GB eMMc+10.1 Inch display.

When the system runs  a period of time,the screen becomes error and black ,IMX6 is crash. The debug UART outputs nothing and can not be input something.

WHY this Problem happen and how to solve it?

Labels (1)
0 Kudos
6 Replies

802 Views
igorpadykov
NXP Employee
NXP Employee

Hi CAI

reason may be ddr errors, so one can test memory with ddr test and

update image with new ddr calibration coefficients found from test

i.MX6/7 DDR Stress Test Tool V3.00 

recommended to use nxp linux releases described on

i.MX Software | NXP 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos

802 Views
897122694
Contributor I

Thanks,igor

we have do DDR stress Test ,and it passed and update image with new ddr calibration coefficients.But the Problem still exists.

Calibration:

MR Value: 0004,
DDR Freq: 365
Stress Test:
StarFreq:200
EndFreq:528

What other way can be check?

0 Kudos

802 Views
igorpadykov
NXP Employee
NXP Employee

what bsp used in the case, please try latest nxp linux releases described on

https://www.nxp.com/support/developer-resources/run-time-software/i.mx-developer-resources/i.mx-6ser...

Best regards
igor

0 Kudos

802 Views
897122694
Contributor I

Hi,igorpadykov:

     I have try to measure the imx6 32.768khz clock and 24MHZ wave.The Vp-p seems not  conforming to the requirements.meet to the picture.

24MHZ:

24mhz1.png

32.768KHZ:

32.768khz2.png

the  requirement is below.

pastedImage_4.png

0 Kudos

802 Views
igorpadykov
NXP Employee
NXP Employee

Hi CAI

one can check clock guidelines provided in i.MX6 System Development User’s Guide

https://www.nxp.com/docs/en/user-guide/IMX6DQ6SDLHDG.pdf

Best regards
igor

0 Kudos

802 Views
897122694
Contributor I

Dear igor,

     BSP used in the case is Android8.0 Linux version 4.9.17,this problem  exist in this case ,but it don't exit in the other item.

0 Kudos